(IE) Danfoss Ireland
Water Controls
 
 
 
 
 
Danfoss Logo

Water Controls - Valves and Flow Control Solutions

Water consumption increases twice at the rate of population growth. Perhaps this valuable resource is not as inexhaustible as men once believed. Today we understand that water is the most precious of gifts.Whatever its purpose, domestic, urban, agricultural or industrial, the water we use every day is distributed by an increasingly complex pattern of pipeline networks.

Danfoss Socla presents type by type a coherent range of complementary devices, wide in scope but specific in application, destined to control the circulation of water and of fluids in general, in the most diverse of installations.

You are about to leave the main www.danfoss.com/ireland and are heading for one of our other business sites.
Danfoss MCD 500 Softstarter

The new intelligent VLT® Soft Starter MCD 500

The Danfoss VLT Soft Starter MCD 500 is a new soft starter in the power range from 7.5 to 800 kW (21 - 1600 A) with sofisticated start- and stopfunctions. 

New in the MCD 500 is the Adaptive Acceleration Control (AAC) function. This function developed by Danfoss adds intelligence to the soft starter. By continuously measuring the motor current and calculating the actual load, the MCD 500 fully automatically adjusts the start and stop profiles to obtain the best possible acceleration and decelaration for your application